AXIS#.LOAD.INERTIA

Description

AXIS#.LOAD.INERTIA is used by Quicktune. If Quicktune is set to a negative value it indicates that the AXIS#.MOTOR.INERTIA keyword may be innacurate and set too high.

Versions

Action Version Notes
Implemented 02-00-00-000
Modified 02-14-04-000 Range expanded to -10.000 from 0.000 minimum

General Information

Type

Read/Write

Units

kgcm² for rotary motors

Range

-10.000 to 1,000,000 kgcm² or kg

Default Value

0 kgcm² or kg

Data Type

Float

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.LOAD.INERTIA

5014h

01h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5700

1

5700 (0x1644)

AXIS1.LOAD.INERTIA

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.LOAD.INERTIA

5700

Float

Read/Write

-